Other Parts Discussed in Thread: CD4051B, TMUX7308F
What happens with other channels if 1 channel is current limited overdriven that diode to supply/gnd is conducting a few mA?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Theory does not help, it must be specified or measured. It seems that I have to order and test samples.
Hello Thomas
So I agree with Clemens in the fact that once the internal esd diode is forward biased( aka when a overvoltage event occurs input signal voltage is higher than supply) and the current exceeds what the diode can handle, then that can cause permanent damage to the device in which TI cannot guarantee correct operation after. I believe this FAQ can explain this in further detail.
However there are devices that have an integrated feature called power off protection that do not have the esd path from input from gnd/supply.
1.Please let me know if that is something that interest you?
2.Also what is the signal that will be causing the overvoltage event in your system?
Please let me know!
Regards,
Kameron
Hello Kameron
thanks. Overvoltage is cause by wrong wiring or short between sensor signals and 24VDC. We have all inputs protected with resistors to limit current and nothing get damaged. But currently we use CD4051 and if 1 channel is overdriven (internal protecting diode conducting) high leakage currents on other channels/output appear. Because we multiplex high impedance sources this cause totally crazy results. As soon as overdrive is removed it works correct again. To avoid this we have to add external overvoltage protection which limit voltages within supply raiils (need many components and cause additional leakage currents of diodes.
best regards
Thomas
Hello Thomas,
Thanks for the extra info,
So I actually recommended you use the TMUX7308F in your design instead of the CD4051B, It power off protection and overvoltage protection which both mean there is no esd path from the io pins to supply/ground. This device should operate in a way that eliminates the high leakage current/measurement error readings you are seeing with the cd4051b. With the TMUX7308F no external protection should be needed.
Please let me know what you think about this device and check out this faq and video for more understanding of why this device should simplify your design.
Please let me know what you think about this new device suggestion!
Regards,
Kameron
Hello Kameron,
yes this would solve issue, same as other instrumentation multiplexer. Also other spces are better but prices are high (about 20 times low cost MUX). We have low cost boards and price would be too high there. I think I´ll make tests to see if it is better than CD4051. At least we can remove the extern level shifter.
best regards
Thomas