Other Parts Discussed in Thread: TMUX6201
HI,
i am driving +/-10 volts input i need SPST Switch i have control voltage 5volts
kindly suggest SPST switch Part no.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
hi logic control voltage i will give 1.8 volts input signal i will drive +/- 12 v this will work. TMUX6201 ac/dc both
i used SPST relay previous circuit now i don't want relay can i use TMUX6201 switch
The TMUX6201 will also work with 1.8 V control signals and 24 V I/O signals
A relay would allow galvanic isolation, i.e., different or floating ground voltages. I do not know if you need that.
Hello Shivaraj,
I agree with Clemens and the TMUX6201 is a good replacement for the relay you previously used in your circuit. It can suppourt 1.8V logic and you can pass +/- 12 v ac or dc signals through the device.
While relays do have a advantage in galvanic isolation, Ti multiplexers Flat ron can provide a more optimized solution than relays
Check out this app note that talks more about replacing relays with multiplexers.
Please let me know if you have any questions
data sheet mentioned +/- 4.5 in my application sending signal low -7 V sine wave peak to peak & high signal 12 volts max for this application i am finding spst Relay
this is my circuit out put side in my application using relay SPST
Hello Shivaraj,
To pass your -7V to 12V peak to peak sinewave signal, you will need to use this device with +/-12V supplies.
This device can pass any signal between it supply ranges of VDD to VSS.
Please let me know if you have any further questions!