This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN74CB3T1G125: Issue when driving A side high while B side has a 10K pull down.

Part Number: SN74CB3T1G125
Other Parts Discussed in Thread: SN74CBTLV1G125

Hi,

We use CB3T1G125 throughout our design as a leakage prevention device instead of level shifting. Basically, we expect this part to be closed when there is power (3.3V) and open when there is no power. We tie the Enable pin to GND - so should be enable always. The 2 sides of the FET are on 2 different power domains but both 3.3V. Each side can be independently on/off.

We are assuming that once the power is on to this device, it is just a 5 OHM series R. I.e. I should be able to drive high and low on one side and see high and low on the other side without any clamping as both sides are 3.3V.

We have seen the following behavior:

With 10K P/D on the B side, when the A side is driven high (3.3V), The B side only goes up to 2.1V.  When we remove the 10K P/D it works fine.

Any idea why?

Thanks

Magid