Other Parts Discussed in Thread: INA827, ADS1261, , TMUX1109
Tool/software:
Hi,
I have designed a schematic for an analog measurement as shown below. On the analog input side, I can also receive negative analog signals from some sensors. The integrated circuits I used are indicated in the block diagram. In this case, to avoid distorting the negative signals coming from the sensor, should I set the supply voltage of the TMUX1209PWR to +5V, GND or +2.5V, -2.5V? I couldn't find any information about the negative voltage supply for the TMUX1209PWR. I would appreciate your insights on this matter. To summarize, I am configuring the analog data received from a thermocouple sensor at the input with a MUX and then transmitting the analog signal from the MUX to the INA827. I am reading the single-ended signal received from the INA827 with the ADS1261.
Best regards.