Other Parts Discussed in Thread: TMUX1574,
Tool/software:
Hello,
I am attempting update a existing test system to be able to run 2 variants of boards. Each variant has its own firmware that needs to be applied via a SD card. Currently the SD card is inside of the fixture, attached via POGO pins to the PCBA and programs with no issues. I created a MUX to allow the system to select what SD card should be used based on the variant. I attached the PCBA via the same POGO pins I am unable to program while using the MUX board inside the fixture.
I fully tested the MUX PCBA at my desk with no issues and I am able to program the board on both sides of the MUX. When installed into the fixture, programming fails, I have removed all other POGO pins expect what is needed to program at my desk to reduce any chance of noise. The failure during programing states it can not access a file. If I take the same board and SD card, I am able to program them by place the SD card directly into the PCBA. I also added the filtering cap between power and ground that the schematic does not show.
Any ideas of what could be causing this, or any additional steps I should take to debug this?