Other Parts Discussed in Thread: TMUX1574
Tool/software:
Do you have a lower Ron/Con than SN74CB3Q3257 w/ TSSOP package ?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Tool/software:
Do you have a lower Ron/Con than SN74CB3Q3257 w/ TSSOP package ?
Hello William,
The best device I can recommend is the TMUX1574. It is p2p replacement with the SN74CB3Q3257 and comes in a TSSOP package.
The TMUX1574 has a typical Ron of 2Ω and typical Con of 7.5pF, while the SN74CB3Q3257 has a typical Ron of 4Ω and typical Con of 10.5pF.
If you are looking for a lower Con/Ron device, we don't have on that is p2p with the SN74CB3Q3257.
Thanks,
Nir