Other Parts Discussed in Thread: TMUX1133, CD74HC4053,
Tool/software:
I need to switch between 2 different negative voltages to the common output.
The negative voltages range between 0V and -1V
1) Can I connect the Vcc to GND, and the Vee to -1.25V (for example) - and then switch between the two voltages?
2) Regarding the select (A) voltage, if it is a square wave driving it (positive polarity source) - can I AC couple it to the A pin?
and I assume I need to give it a DC voltage reference to the middle point desired. would a voltage divider of 1K and 1K from Vee to GND work? and do I need an AC coupled 50 ohm for a fast square wave?