This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TS5A3167: why previous output reflects even after changing the control logic to 1

Part Number: TS5A3167
Other Parts Discussed in Thread: SN74LVC1G07

Tool/software:

Hi,

I gave +5V to supply pin.

Input of the channel = 5V.

when the control logic Low = 0V, I got 5V at the output of the channel/switch.

But when I changed the control logic to High = 5V, then also I am getting 5V at the output, i.e the previous output remains at the output even after changing the control logic,

whereas i expect high impedance and hence no voltage there, as the switch is open now for logic 1.

My application requirement is,

for Logic 0 : Input of the channel, i.e 0V or 5V or specifically a short to ground.

for Logic 1: Open or High impedance

Please help me out to solve this. or suggest some other Texas IC to meet my requirement.

Thanks & Regards,

Indira