Other Parts Discussed in Thread: TMUX1072, TMUX4053
Tool/software:
I have looked through all yours multiplexers and competions, the best and almost only choice to fullfill our requirement in function, very low capacity, supply voltage, size and price is the TMUX136.
Its primary use case is digital, but I will use it for analog signals. Multiplexers intented for analog use normally have an ACPSRR spec of say 40dB, TMUX136 datasheet do not.
Our frequency range for PSRR is only from 10K to about 10MHz, anythink lower or higher is don't care. Can you provide any information of PSRR we can expect?
Is the internal construction of the TMUX136 different from analog muxes. is there a mux with similar internal construct that has a PSRR spec?
We also want to know if there can be coupling from the SEL pin to signal?
The noise signals on power and SEL will be below 10uV. We want the coupled noise on the A/B/COMMON to be significant lower like <100nV!