This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMUX1308A-Q1: Is TMUX1308A-Q1 ok for Lidar PWM gate driver

Part Number: TMUX1308A-Q1
Other Parts Discussed in Thread: LMG1025-Q1

Tool/software:

Hi BU team

My customer is developing the multi-line flash Lidar application. TMUX1308A-Q1+n*LMG1025-Q1 drive the PMW signals to MOSs. 

The PWM waveform is shown in below screenshot. 

The pulse width is 5ns , the pwm frequencty is about 2MHz( duty cycle is 0.046%), trising=307ps (20%-80%),tfalling=287ps (20%-80%). 

Is TMUX1308A-Q1 ok for this application? if not, what's your suggestion on new solution with automotive level?

Thanks