Part Number: TMUX1072
Tool/software:
Hi team,
Could you please help check the application of TMUX1072?
1. Device VCC = 3.3V
2. IO input and output level is 1.8V
3. Whether the application signal supports MDIO protocol communication and the communication rate is 2.5M,
4. Whether bidirectional communication is possible?
I find in the datasheet that the IO voltage should be higher than VCC and lower than 5.5V, so does it mean that TMUX1072 cannot work under this condition?
If it cannot, could you please help recommend the most suitable socket?
Thanks a lot!