Other Parts Discussed in Thread: LMK00101, LMK00105,
Tool/software:
I plan to drive the A input with a square wave of 160MHz to switch the inputs between Y1 and Y2.
the source of this signal will be LMK00101 in one configuration, and LMK00105 in the other.
both have 50 ohm source impedance LVCMOS outputs.
I expect the lines to be approx 5 to 10cm long.
I understand the voltages are suitable to drive the A input on the SN74AUC2G53 and presumably should DC couple?
What is the input impedance of the A input?
Do I use 50 ohm (or some other impedance) transmission line from the LMK to the SN74AUC2G53 A input?
Do I need to add anything for termination of the line into A in order to get a clean switch? I assume 50 ohm to GND (virtual GND, I am using -2.5V as Vee and GND as Vcc for the LMK as well and the SN74AUC2G53) would draw too much current from the LMK LVCMOS fanout? I thought maybe I need a 50 ohm in series with 0.1uF to Vcc or Vee?
Or perhaps nothing is needed? (will be happy to avoid extra parts in a crowded area - and I have a few of these switches...)
All spec and advice welcome
thanks
Pinhas