This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMUX8212: Can I power the TMUX8212 with only a negative supply?

Part Number: TMUX8212
Other Parts Discussed in Thread: TXG1041, LM2665

Tool/software:

Hi TI Team;

Can I power the TMUX8212 with only a negative supply? I would like switch negative voltages.

Example: VDD = 0V; VSS = -36V

If that is not possible, can I power it with a positive voltage that is lower in absolute value than the negative voltage?

Example: VDD = +5V; VSS = -36V

Thanks in advance.