Part Number: TPS552892
Tool/software:
Hi,
We are using a TI buck-boost IC, TPS552892, and have encountered an issue with unstable power compensation, as shown in <Figure 1> and <Figure 2>. Ultimately, due to excessive peak current triggering the protection component, the power source was disconnected.
The circuit diagram is shown in <Figure 3>, and it is essentially configured according to the EVM setup.
The input and output voltages are both 12V, with a current transient of approximately 100mA to 1.5A.
- Have you encountered this issue before, and what might be the possible causes?
- Would increasing the switching frequency (Fsw) to improve response speed effectively stabilize the output voltage in a timely manner?
- We are now planning to adjust the Fsw frequency to 1.2MHz (15kΩ). For the frequency response, do you have any recommended values for the components R1440/R1568/C1569/L19 in <Figure 3>?
- I have tried to using webebch tool to design for 1.2Mhz, but why only can choose 0.2 - 1.067Mhz? Is it webebch tool bug?
Figure 1

Figure 2

Figure 3

Thanks!
Jeff