Part Number: TMUX8212
Other Parts Discussed in Thread: TMUX7411F, TMUX7412F, TMUX7413F, TMUX7462F, TMUX7436F, OPA2992, LM741, TVS1800, TVS1801
Tool/software:
I'm using a TMUX8212 in a design that requires the board's outputs be clamped to ~20V. Previously we had thought that we'd use a lot of Zener Diodes that would be able to clamp but since the Analog Switch uses CMOS I thought that we'd be able to simply make the rails of the switch ~25V such that it's on-resistance is still low but if there are transients in the signal line they would be clamped to the rails.
I created a schematic where I have all inputs hooked up to a sinusoidal voltage source with amplitude at ~30V and then set all the select lines HIGH expecting that the output would be a clamped sinusoid with a maximum of ~25V.*** Instead I'm having issues with TVS Diodes and other Diodes that's causing divergence in simulation results and resulting in what seems like infinite current. Not sure if this is causing all the issues or simply a result of whatever is going on in the simulation. Not sure if this is an accurate representation of the device but seems odd to me since the issue only appears after 1V over the rails. (e.g. Whenever the rails are ~25V and inputs are ~26V then there are no issues.)
I'm interested if the device is able to function as this or if I should use the multiple Zener Diodes on the inputs or outputs.
Thanks for the assistance and let me know if there is more information that I can provide.
*** I'm unable to share the schematic and results as a result of the computer that it was created on - but can describe it. Thanks!