Part Number: TMUX8212
Tool/software:
My signal is a sine wave with a voltage of ± 30V, 10MHz, and the load is ~30 Ω, so the current is ~ ± 1A. The signal is periodic and lasts for 5 cycles each time, followed by an interval of 50ms before another 5 cycles. I see that the maximum single channel of the drain pulse current source is 560mA. Can it support my 1A periodic signal? If not, Can I connect two or three channels together to this signal in parallel. Is there any problem with connecting this signal, or are there any other chips that support high current? Thanks