Other Parts Discussed in Thread: SN74CB3T3245
Tool/software:
背景:使用SN74CBT3245C作为电平转换电路,一端要求5V,另外一端要求3.3V,支持双向通信,5V侧通过4.7K电阻上拉到5V,3.3V侧接入FPGA控制芯片。
1、SN74CBT3245C供电VCC看规格书输出侧会比VCC小1V,因此通常使用5V接二极管后给VCC供电,目前我验证VCC=4.3V,但输出侧在3.5V左右并不是3.3V,而且输出侧悬空和接入FPGA两者值不一样,且4.7K上拉电阻上接近0.5V压降,应该是存在电流通路,请问这个电流怎么评估?VCC供电为什么要使用二极管压降减少的形式?VCC供电可使用电阻分压或者431电路吗?
2、5V输出侧悬空,为什么上拉电阻4.7K上还会存在0.5V压降,是通过输入进到了FPGA里面形成电流通路?而且我把4.7K电阻改成1k,压降会相应的减少到0.1V左右,感觉电流是差不多恒定的,这个压降不可避免?