This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TS5A3159A switching issue



Hello,

We have an issue with the TS5A3159AYZPR where it is basically used as a tri-state buffer.  Normally Open (NO) is tied to a CPLD signal this is used a Chip Select for a battery backed SRAM.  NC is left floating, and IN is tied to a voltage level detect circuit that monitors if main power is present, or if the system should switch to the backup battery.  V+ is tied to a 3.3V rail produced by main power.   The thought was that as main power is lost, IN would go low, switching NC to COM, turning it into a high-Z line.  The CS_N (COM)  is pulled high through a 10k to Vbackup battery (3V). 

Instead, the COM seems to follow V+ and NO slowly down until power is almost completely gone.  This is causing the CS_N to fall briefly and corrupting the first byte of the memory.  We've tried holding IN low while V+ is still fully powered, and then removing power.  COM falls a little faster, but still isn't high impedence until V+ is really low. 

Is there something internal to the part that would prevent an open NC pin from looking like a high-Z line when connected to COM? or anything else that could explain this performance?

Thanks,
Eric