Hello Signal Switches forum, do we have any SPST switches with an on-resistance less than 5 ohms? Small package is preferred
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello Signal Switches forum, do we have any SPST switches with an on-resistance less than 5 ohms? Small package is preferred
Yes we have several SPST switches with typical on resistances around 5 ohms or less. I have provided a list of devices below.
Part Number | Mux Configuration | Switch Configuration | Channel(s) count | Analog Signal (min) (V) | Analog Signal (max) (V) | Supply Voltage min (V) | Supply Voltage max (V) | I/O continuous Current (max) (mA) | I/O peak Current (max) (mA) | Icc max (uA) full temp | Icc typ (uA) | Ron typ (Ω) | Ron max (Ω) full temp | Bandwidth typ (MHz) | Features |
TS12A4515 | 1:1 | SPST | 1 | 0 | 12 | 0 | 13 | 20 | 30 | 0.2 | 0.05 | 6.5 | 50 | 520 | Single Supply Break before Make |
TS12A4514 | 1:1 | SPST | 1 | 0 | 12 | 0 | 13 | 20 | 30 | 0.2 | 0.05 | 6.5 | 50 | 520 | Single Supply Break before Make |
TS3A4741 | 1:1 | SPST | 2 | 0 | 4 | 0 | 4 | 100 | 200 | 0.75 | 0.05 | 0.7 | 2 | 125 | Single Supply |
TS3A4742 | 1:1 | SPST | 2 | 0 | 4 | 0 | 4 | 100 | 200 | 0.75 | 0.05 | 0.7 | 2 | 125 | Single Supply |
TS5A21366 | 1:1 | SPST | 2 | 0 | 5.5 | 0 | 6.5 | 200 | 400 | 10 | 3.6 | 0.75 | 5 | 260 | Single Supply USB 2.0 |
TS12A44515 | 1:1 | SPST | 4 | 0 | 13 | 0 | 13 | 20 | 30 | 200 | 30 | 6.5 | 50 | 530 | Single Supply USB 2.0 |
TS12A44514 | 1:1 | SPST | 4 | 0 | 13 | 0 | 13 | 20 | 30 | 200 | 30 | 6.5 | 50 | 530 | Single Supply USB 2.0 |
TS12A44513 | 1:1 | SPST | 4 | 0 | 13 | 0 | 13 | 20 | 30 | 200 | 30 | 6.5 | 50 | 530 | Single Supply USB 2.0 |
TS3A4751 | 1:1 | SPST | 4 | 0 | 4 | 0 | 4 | 100 | 200 | 0.75 | 0.075 | 0.7 | 2 | 125 | Single Supply |
Thank you,
Adam