Other Parts Discussed in Thread: SN74CB3T1G125, SN74CB3T3245
Hello,
Can you look at the following datasheet discrepancy?
This is the functionality note for the single version of the CB3T family - SN74CB3T1G125:
NOTE A: If the input high voltage (VIH) level is greater than or equal to VCC – 1 V, and less than or equal to 5.5 V, then the output high voltage (VOH) level will be equal to approximately the VCC voltage level.
This is the functionality note for the octal version of the CB3T family - SN74CB3T3245:
If the input high voltage (VIH) level is greater than or equal to VCC + 1V, and less than or equal to 5.5V, the output high voltage (VOH) level will be equal to approximately the VCC voltage level.
Just wondering if this is a misprint? -1V and the other is +1V? Which is correct?
Thanks!
Paul