Hi,
A CD4066BE is a CMOS that comes with four bilateral switches, and I was wondering if there is a way to turn on all the switches to run, for instance, a motor?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
A CD4066BE is a CMOS that comes with four bilateral switches, and I was wondering if there is a way to turn on all the switches to run, for instance, a motor?
Hello Adam,
I found this switch TS12A44513 which I really need but the problem with that is the Package Group comes only on SOIC and TSSOP and what I need is PDIP or CDIP so it can fits my bread board. So if there is any switch with the same specifications of TS12A44513 and has a Package Group of PDIP or CDIP? Also, if it is possible to have a VCC (Max) of 15V?
I am looking forward for your feedback. Thanks
Alhawsawi,
I filtered the analog switch selections by your package requirements.
You can use 4 TS12A4515 devices that are similar to the TS12A44513 but in the package you need.
You could also order a break out board that can interface the TS12A44153 device to a bread board. I have used a company called proto advantage in the past who will solder the devices you want on a small PCB will DIP headers for a couple of dollars and I'm sure there are plenty of other companies around the world that provide the same service.
We don't have too many switches that operate above 12V at the moment but we would love to learn the reason why you would want that feature so we can think about building these types of parts in the future.
Thank you,
Adam