The TS12A12511 features a 5V logic level input suggesting that it will operate from signals having a nominal 0 to 5V swing typical of logic circuits supplied from 5V regulated sources. However, the regulators for those circuits have tolerances on their output voltages which could result in the supply voltages being under 5V. There would then be uncertainty as to whether the switch would operate when it is supplied with 12V since its upper limit switch threshold is then specified at 5V. Is the specification in error? Should the upper limit threshold be something under 5V so that a 5V input signal will ALWAYS WORK WITH ALL OF THE PARTS?