Hi, I'm using TS5A3167 analog switch.
Can I input some positive voltage analog signal to NC or COM while V+ is 0V?
Although the absolute maximum rating of analog input is "(V+) + 0.5V" in the datasheet, the note (4) says "it may be exceeded if the cramp current is observed". The abs max of Analog input current is only "-50mA" and no positive value are written.
Does it mean I can input "0 + 0.5 V" signal to NC or COM when V+ = 0V?
I think listing only "-50mA" implies no diodes are between input and V+.
If so, is the abs max input of "(V+) + 0.5V" correct?
Thanks,