Hello,
One of my customers have used the Fairchild IC - FST3257 in their projects and recently they decided to replace it to a direct replacement from TI - the SN74CBT3257C. They have 3 ICs of the FST3257 in their board and the design used to work for them with the Fairchild ICs. With our IC they have a problem and the IC (U11) is burning when they use TI chip instead of the Fairchild chip. Can you please inspect the attached schematics and let us know what is the cause of this issue? are there any differences between the two chips?
P.S VBS is 5.4V
Regards,
Meir.