Other Parts Discussed in Thread: SN74CB3T3253
Hi all
Would you mind if we ask SN74LV4051A?
What is "Support Mixed-Mode Voltage Operation on All Ports" used for?
It is not tolerance function, right?
Our customer would like to use following conditions.
(We guess that our customer misunderstands "Support Mixed-Mode Voltage Operation on All Ports".)
<Condition>
-Y0~7 : 5.0V level
-COM : 3.3V level
Vcc : 3.3V
->Recommended Input or output voltage is upto Vcc(in this case 3.3V).
So, it will be over Absoulute Maximum, that's why this is NG.
Is our recognition correct?
Kind regards,
Hirotaka Matsumoto