This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TS3A27518E: Switch solution for SDIO 3.0

Part Number: TS3A27518E


From email:

----

My customer is currently looking at some SDIO 3.0 (up to 208MHz for SDR104) Multiplexing solutions. Our TS3A27518E might fit the bill but not sure about BW - can you please confirm?

 

If not, can you help in recommending a more suitable part?

 

Please let me know – it’s a pretty urgent matter.

---

Regards,

Sonia

  • Hello Sonia,

    I did a quick check on the SDIO standard mentioned (SDR104) and pulled this snippet to confirm the BW required at the specific voltage level (circled in blue):

    I have also attached the pdf for more information about this standard below:

    As for our solution, TS3A27518E, assuming BW at 1.8V is the only concern your customer has, then yes, according the snippet from the TS3A27518E datasheet, you should be fine, with a about 30MHz to spare (highlighted):

    Thank you,

    Louie

    If I have answered your questions, please hit Verify Answer.