This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TSU6111: Default switch state when ADC indicates "11111"

Expert 4840 points
Part Number: TSU6111


Dear e2e community,

When when my customer connects a usb cable, the ADC value indicates "11111". The switch seems to be in open state at that time.

As there are 4 possible Switch States, for this ADC value, which one should we consider at the initialization?
In ohter worlds, what is the default switch state (USB/UART or OPEN?) when ADC indicates "11111"?

Device Type 1 and Device Type 2 registers = 0x00

Regards,