Other Parts Discussed in Thread: SN74CB3Q3253, , TCA9800
Hi
Do unused analog inputs need to be pulled to GND or VCC via resistor (fro SN74CB3Q3251 and SN74CB3Q3253)
If so is this required for
a) Device protection e.g. latchup
b) Noise immunity.
c) Both
Also , what would a reasonable (max) value be.
In my application some of the analog inputs/outputs may or may not be connected to "devices".
If the devices are present (or powered) they have constant current source pull ups on them so it is
not advised to connect external PU's (device in question is TCA9800 I2C level translating I2C Buffer/repeater
- B side connections).
Finbarr