This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN74CBTLV1G125: SN74CBTLV1G125

Part Number: SN74CBTLV1G125
Other Parts Discussed in Thread: TS5A21366

hi all,

 The part number above mentioned is a LOW-VOLTAGE SINGLE FET BUS SWITCH , has the  High-level control input voltage of 1.7v , can anyone suggest any part which should have the High-level control input voltage of 1.2v

  • Manoj,

    We have FET switches that can support High-level control input voltage of 1.2 V.  What do you think about using the TS5A21366?

    Why do you need to use 1.2 V as your control input voltage threshold?  What power supply voltage do you want for the IC?

    Thank you,

    Adam