Other Parts Discussed in Thread: BQ24075
I want to know the current consumption when COM is connected to NC and when it is connected to NO. Is it the same current consumed by the IC or different values. What I think is that when COM is connected to NC it should not consume any current as it is in NC state and it should consume current only when COM is connected to NO pin. It also says in the datasheet that it consumes 100mA continuous current through V+. Shall I consider this current or a different current.
Thanks