Part Number: CD74HC4051-Q1
Other Parts Discussed in Thread: CD74HCT4051-Q1
Hi Team
may I get your reply on the below ?
thanks.
[Q1] CD74HC4051-Q1 can bi-directional transfer analog signal in the range of ± 6V by VCC ~ VEE pins by setting VCC = +6V and VEE = ─6V.
However, the control input signals for S0/S1/S2/E pins must be in the range of 0V ~ 6V by setting VCC = 6V and GND = 0V.
Am I right ?
[Q2] If the bidirectional signal is within 0V ~ 5V range, we should provide VCC = 5V and VEE = 0V.
In this case, can we connect GND pin and VEE pin directly together ?
[Q3] If the bidirectional signal is within ─2V ~ 5V range, we should provide VCC = 5V and VEE = ─2V.
In this case, GND pin will be 0V. under such situation, can we connect GND pin through capacitance to VEE pin ?
If that how much cap value is OK ?
Or we should not connect GND pin through any Cap to VEE ?
Just I want to know our recommendation for this case.
[Q4] what it the Max possible Switching Frequency for S0/S1/S2 pins ?
[Q5] the transferable Min frequency(= -3dB) for A0~A7/COMOUT pins are 180 MHz at ± 4.5V for VCC ~ VEE ?