Other Parts Discussed in Thread: TS3A44159, TS3A5018, SN74CB3Q3257, TS5A3359, SN74CBTLV3253
Hi Support Team,
I am going to to use SN74CB3T3257 to switch the signal from the Tester channels (TC) to two devices (DUT), please help to support on the following questions:
1. The chip is powered by 3.3V, but 1.8V would be the logic interface between TC and DUT, please help to confirm if this is OK?
2. The clock signal will pass through the chip, any problem at 200Mhz?
3. The signals include both input and output, please let me know if any propagation delay when then the signal travel in bio-direction?
4. I also found another chip - TS3A44159 that would be suitable for my application. Any comparison between the SN74CB3T3257 and TS3A44159, which one is better for my application (as above: logic voltage, speed, delay...)?
5. My application need at least 50 ICs for all signals switching, Any recommendation for power supply and logic control selection in-out...? For example: the whole CHIP will be powered by 3.3V@400mA; each 10 pins (S) will be control by 1 relays (combine two form of G6K-2P-Y DC3 relay to H via 10K to 3.3V and L via 470R to GND; all EN pins will be tie L (GND). If use either SN74CB3T3257 or TS3A44159, is this design OK?
Thanks You,
Phuc Le.