Other Parts Discussed in Thread: SN74CBTD3306
Hi there:
Our customer would like to check the detail parameter of SN74CBTD3306C
such as OE# pin's threshold voltage range.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi there:
Our customer would like to check the detail parameter of SN74CBTD3306C
such as OE# pin's threshold voltage range.
Hi Dakotah:
thanks for the information
update application from customer
The reason of checking Vth about SN74CBTD3306:
an spike voltage (under 0V ) happened in 1A/2A pin, what's the accept voltage range for this pin will not trigger the 1B/2B (not happened with SN74CBTD3306C) ?
schematic
waveform (not SN74CBTD3306)
Hi Kay,
I am a bit confused by your question.
If I am interpreting it correctly the customer is looking into two devices: the SN74CBTD3306 and SN74CBTD3306C.
If the custumer system has a negative voltage spike on the signal path, the correct part to use is the SN74CBTD3306C. This device supports -2V undershoot operation. Please reference the following application note for more on the undershoot protection of the "-C" devices. 
Eric,
The SN74CBTD3306 can support voltages as low as GND on the signal path to be within the recommended operating range.
If you need the negative undershoot protection the SN74CBTD3306C is the correct part.