Other Parts Discussed in Thread: SN74CB3Q3384A
Hi,
Since there is no information of VOH, VOL in the data sheet of SN74CBT3384A, we refer to scdd001b.
Application notes (scdd001b) 9-7 (page 355)
It has the following description.
"The transistor clamps the output at ≈1V less than the gate potential, regardless of the level at the input pin."
I have a question.
How much does the potential of about 1V vary? (error)
For example, dropping 0.9V or dropping 1.1V.
best regards
cafain