Hello Team;
Our Customer pointing out that Outside Dimension of DSBGA are two different size, and would like to confirm these figure are correct or not?
www.ti.com/.../scds187c.pdf
1) On top page, "Device information" Dody side as "DSBGA 1.50 mm x 0.90 mm"
2) On page 28., Dimension are written as following.
D: Max = 1.418 mm, Min = 1.358 mm
E: Max = 0.918 mm, Min = 0.858 mm
The D size on top page is 1.50 mm(Typ), but actual size is smaller than 1.418 mm, even this figure are Maximum" size.
Customer pointing out that "This is error".
Can you explain why?
Thanks.
Masaru Shigeta - Japan CSC