Other Parts Discussed in Thread: SN74LV4053A-Q1, SN74HC4852-Q1
Hi,
I'm looking into TI analog mux portfolio for multiplexing multiple NTC temperature sensors into 1 or 2 ADC input channel of a MCU. Right now I have SN74LV4053A-Q1, SN74HC4851-Q1 and SN74HC4852-Q1 in mind.
4051 does not specified the 'injection-current effect control' features and the maximum input clamp current rating is in negative. Is the clamp current flow through the internal ESD circuitry when the analog terminal swing below GND? Also, for any circumstances that analog terminal swing above Vcc, a external diode clamp to supply rail is necessary, right?
Besides, from the Fig. 4 of 4851 and 4852 datasheet, I could tell that an intrinsic diode eliminates the need for external clamp outside the analog terminal. Are there any ESD circuitry between the analog terminals and GND?
Great thanks for your help!