I had a question regarding the following part: SN74CBT3384C . On the datasheet, Digital Input LOGIC HIGH starts at 2 V. Logic LOW ends at 0.8 V. Would it be possible to use this part as a level shifter (input 3.3V to drive a 5V circuit) since the part would interpret a 3.3 V signal input as LOGIC HIGH?
Image taken from: https://www.ti.com/lit/ds/symlink/sn74cbt3384c.pdf