Part Number: TS5A21366
Hi TI experts,
For current project I'm evaluating using TS5A21366 to isolate the ADC signal from potentiometer to uController.
However I want to know if I can use only one control signal for IN1 & IN2.
Is this possible or is there any internal circuitry that I need to pay attention to?
Externally there is a pull down resistor 10K on the control signal for another PowerFET circuitry control.
Basically I wanted to use single signal to toggle the MOSFET and TS5A21366 if possible.