Other Parts Discussed in Thread: SN74CBTLV3245A, SN74CB3Q3244
Hi Experts:
Customer use SN74CBT3244 as switch in PDB, enable signal is FM_SLED_PWRGD and circuit as below.
And they found the SMB_PSU_PMBUS_ALRT_N (pin5) of U2 only got 2.5V output but the source pin is 3.3V.
I removed all end device of SMB_PSU_PMBUS_ALRT_N<0>, and the voltage still 2.5V.
Do you know why the voltage will go lower than input side? Do we need to add external pull-up on the output side?
But SN74CBT3244 should be a push pull output, i don't think we need pull up resistor at output, right?
Thanks.