Other Parts Discussed in Thread: SN74CBTLV3126
Do you have a device that is P2P compatible with SN74CBTLV3126PWR but 1.8V VIH?
Do you have suitable tool to filter all of the logic components?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Do you have a device that is P2P compatible with SN74CBTLV3126PWR but 1.8V VIH?
Do you have suitable tool to filter all of the logic components?
Whitney,
Yes, the TMUX1511 is p2p compatible with the SN74CBTLV3126. The key differences are the TMUX1511 will support 1.8V logic signals and it has a wider supply voltage range which gives designers more flexibility to use different power rails and on different projects.
The TMUX1511 device is good for digital signaling applications like SPI or JTAG bus isolation.
Yes, there is switch selection tool I used to find the TMUX1511 device on ti.com. I filtered for 1:1, 4-channel, to find the device I needed.
Thank you,
Adam