This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMUX1204: Isolation at Vdd = 0

Part Number: TMUX1204
Other Parts Discussed in Thread: TS3A5017

Does the TMUX1204 provide isolation if Vdd=0? If not, could you provide another 4:1 mux with this isolation and Ron < 30 Ohms?

Looking at the TMUX1204 datasheet it seems like it only provides control pin protection, as in if the control pins are powered before VDD, then the rest of the chip is protected. I am mainly interested in isolating the output of the MUX when Vdd=0.