This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMUX1208: Need an comparable automotive device to TMUX1208

Part Number: TMUX1208


Hello all,

I'm searching for an automotive device similar to TMUX1208. 1.8V compatible, with wide supply range.

Best Regards,

Matt

  • Matthew, 

    We currently do not have an 8:1 device with 1.8 V compatible logic and wide supply range that is automotive qualified.  We are always looking for ways to better serve our customers and will bring this request to our product definers.  Do you know what type of package you would like to have for this type of switch?  What is driving the need to have a wide supply range? 

    Thank you,

    Adam

  • Hello,

    This was a one-off case where I wanted to avoid using a I/O port expander (due to cost), and use a multiplexer with my 4 available I/Os on my serializer to provide control to the MUX that would expand my I/O count to 8 (basically 3 serializer for control, and one as universal input).  The end equipment is a camera module where the serializer only operates on 1.8V. The mux posted above is 1/4 cost of expander so was hoping for the option.

    Thanks again,

    Matt