This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TS12A4514: looking for similar device such as ADG1401

Part Number: TS12A4514

Hi team,

I have the needs to control 1:1 SPST analog switch to drive 12V 30mA (Continuous current) LED with TTL (3.3v) digital input (like ADG1401).

in the TS12A4514 Datasheet the Continuous current is not clear to me (what mean -+20mA), could you please advise what is the Continuous current at TS12A4514, in my application I need at least 30mA.

please advise if there is another device which can be suited for my application.

Thanks and regards,

Shai