This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN74CBTLV1G125: question on the DATASHEET

Part Number: SN74CBTLV1G125

Hi,

I have a question regarding this part,

The datasheet specifies a VinHighMin of 2V when supplied at 3V3.

We assume the A to B connection are 2 FET switches so it should not care about high or low as it is just an analogue connection. The VIN levels should only be applicable on the OEn input, but the datasheet is not clear on that.

Are these assumptions correct and can we connect an LVCMOS18 signal to the A-port of the device?

The device will be supplied by 3V3, OEn will be tied to GND.

Thanks and regards.

--