This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TS5A2066: Could you please suggest the 1:1 switch candidate which is suitable for microphone PDM signal?

Part Number: TS5A2066


Hi Sir,

For customer application, they would like to add a switch for camera module... when camera off then microphone module need to be off at the same time.

So, they need a 1:1 switch for PDM signal (CLK/DATA), the clock frequency should upper to 4.8MHz and supply should be 1.8V or 3.3V.

I am not sure the TS5A2066 will be suitable candidate or could you suggest a candidate for 1:1 switch which is suitable for PDM or I2S signal?

Thanks,

George