Hi Sir
I saw ADI mux solution have "latch-up proof" function
is it the same function for "Latch-Up Performance Meets 100 mA per JESD78 Class II Level A on all Pin"
May I know latch up function's benefit ?
Thanks
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello,
Thank you for your question. Our team is currently on holiday, so you can expect a response from someone on our team on Monday, December 2nd.
Best regards!
Hi Kai,
Latch-Up is a condition where a low impedance path is created between a supply pin and ground. This condition is caused by a trigger (current injection or overvoltage), but once activated, the low impedance path remains even after the trigger is no longer present. . Latch-Up is not a risk if the voltage and current levels applied to the device adhere to the absolute maximum ratings.
The "Latch-Up Performance Meets 100 mA per JESD78 Class II Level A on all Pin" means that the TMUX6136 will protect up to 100mA during latch-up.
Can you explain your use case and how much latch up protection you need?
Regards
Saminah