Other Parts Discussed in Thread: OPA192, TS12A12511
Dear All,
I am going to design one 8 Channel Data Aquistion Project.
The input details are given below:
1. Each Channel analog input with selectable range ( ± 5V or ±10V ) of Single Ended input.
2. Input Impedence 1M Ohm
3. Input is DC Coupling.
Here is My block diagram is attached below.
Here Op-Amp OPA192 is used for Buffering the Input . The output of OPA192 is directly Connected to one input of TMUX6119
and Divider output of OPA192 is connected with Another Input of TMUX6119. Through MUX ic we are selecting ± 5V input from OPA192 or ±10V input from voltage divider.
The TMUX6119 selection is Controledl by MicroController / FPGA.
Due to Transmission Gate( TMUX6119 ) Whether voltage divider reistor input will affect the passive low pass filter response?
Please give your suggestion .
Regards
Lakshmanan V