Other Parts Discussed in Thread: TMUX1109, TMUX1133, TMUX1134
Tool/software: Code Composer Studio
Hello, I need to generate a Tri-Level Sync Pulse:
From Wikipedia:
The main pulse definition is as follows: a negative-going pulse of 300 mV lasting 40 sample clocks followed by a positive-going pulse of 300 mV lasting 40 sample clocks. The allowed rise/fall time for each of the transitions is 4 sample clocks. This is with a clock rate of 74.25 MHz
I'm looking at the CD4053 device and looking in the datasheet for the min/max on the analog inputs. I intend to connect -300mV to A and +300mV to B. I will connect ay and by together and run the sum through an RC low-pass filter. I trying to find in the datasheet the min/max voltage on the inputs A/B/C.
Can you help me? Also if there is a better device please let me know.
Thanks,
Joe