This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN3257-Q1: Avoiding a level shifter

Part Number: SN3257-Q1
Other Parts Discussed in Thread: SN74CB3T3257

Hi,

I would ask you for information about the operation of SN3257-Q1.

If powered at 3.3V, if on S1A, S1B there is a CMOS signal that switches between 0 and 1.8V, on D1, the logical value 1 is 1.8V or 3.3V?

I need to know, to avoid a level shifter. Being a mosfet with 5Ohm of resistance I expect 1.8V also on D1, is it correct? Or is the MOSFET off when there is a '1' so I will have 3.3V at the output?

If you can get the information it would be useful, otherwise I have to insert a level shifter.

Many Thanks,

Antonio