Other Parts Discussed in Thread: SN74CBT3257C, SN74CB3Q3257
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
The recommended operation conditions of the SN74CB3T3257 do not allow a supply voltage larger than 3.6 V, and it clamps its outputs to its own VCC. You should not use the SN74CB3T3257 if you do not actually want level shifting.
Just use a plain 5 V mux like the SN74CBT3257C. Its datasheet says:
This device is fully specified for partial-power-down applications using Ioff. The Ioff feature ensures that damaging current will not backflow through the device when it is powered down. The device has isolation during power off.
Please note that Ioff works only if the power supply is at 0 V, not when it's floating.
1. The absolute maximum ratings and recommended operating conditions allow this.
2. That is prevented by the Ioff feature.
Hello,
1. For protection when voltage is applied to the control input pins when Vcc = 0V is typically referred to as fail-safe logic. You can learn more about this feature in this TI Precision Labs training video.
2. For protection when voltage is applied to the I/O signal pins when Vcc = 0V is typically referred to as powered-off protection. You can learn more about this feature in this TI Precision Labs training video.
To confirm, do you need to pass 5.5V I/O signals while Vcc = 2.5V? If so, we need to find a device that supports input/output voltage beyond supply.
Have you looked at SN74CB3Q3257?
Best regards,
Kate
Thank you for your reply.
>To confirm, do you need to pass 5.5V I/O signals >while Vcc = 2.5V?
Yes.
It seems SN74CB3Q3257 meets my request.
In this case, it operates normally at Vcc = 2.5V, and there is no problem if 5.5V is applied to the signal line when Vcc = 0V, right?
Let me confirm that my understanding is correct.
Basically, if there is an Ioff function, there is no problem even if 5.5 V is applied to the signal line with Vcc = 0.
However, depending on the maximum rating of the data sheet and the recommended operating conditions, if it is described on the assumption that Vcc is applied to the recommended operating conditions such as SN74CB3T3257, apply a 5.5 V signal with Vcc at 0 V It is not possible.
Hello,
SN74CB3Q3257 is my recommendation for the following reasons:
>>"Basically, if there is an Ioff function, there is no problem even if 5.5 V is applied to the signal line with Vcc = 0."
If there is an Ioff specification (OFF leakage current) at the test condition of Vcc = 0V, the switch has powered-off protection (as indicated in my previous point).
This specification also indicates that the switch is protected with I/O voltage up to 5.5V. This value may vary depending on the device and is indicated in the datasheet.
Best regards,
Kate
Sorry for writing continuously.
Please tell me additionally.
④ When Vcc = 0V, does the SN74CB3Q3257 guarantee power-off protection up to 5.5V regardless of whether OE is 1 or 0?
Hi,
Thank you for consolidating your questions to your single most recent post. You can expect a response from our team on that thread!